• No : 20929
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800-R2R

What is the proper use of using the tension controller and using the FR-A800-R2R?
Category : 

Answer

The tension controller is suitable for the equipment with low speed and small capacity. The tension controller is suitable for the equipment with low speed and small capacity.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800 Plus