• No : 20932
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800-CRN

Is it necessary to set the rope length every time the anti-sway control is performed and the rope length fluctuates?
Category : 

Answer

Yes, it is preferred. The accuracy becomes worse when the gap between the setting value and actual value increases.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800 Plus