- No : 20945
- Release Date : 2018/08/22 16:25
-
Print
Input phase loss protection
Why is the initial value of Pr.872 (Input phase loss protection) "1" (Valid) for the A701 and "0" (Invalid) for the A700?
- Category :
-
Answer
The initial value of Pr.872 is set to "1" (Valid) because the A701 have regeneration unit built-in and an overvoltage may occur when the regenerative operation is performed at an input phase loss.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700