• No : 20998
  • Release Date : 2018/08/22 16:25
  • Print

Communication specifications for connection of multiple inverters

When connecting multiple A series/F series inverters, what terminal should I use for the communication?
Category : 

Answer

Use the RS485 terminal for the multiple communication of the A series/F series inverters.* Communication with the PU connector is only one-to-one connection.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800