• No : 21002
  • Release Date : 2018/08/22 16:25
  • Print

FR-A8AP

When the 24 V complementary type encoder is used, what is the voltage level at ON and OFF of the A8AP?
Category : 

Answer

The ON level is the power supply voltage -3 V or higher and the OFF level is 3 V or lower.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
Option