- No : 21011
- Release Date : 2018/08/22 16:25
-
Print
FR-A701
Can I connect the reactor for the harmonic suppression to the FR-A701?
- Category :
-
Answer
The AC reactor (FR-HAL) is built in the FR-A701. (The circuit type in the Harmonic Suppression Guidelines is three-phase bridge (capacitor smoothed), with reactor (AC side).) The connection with the stand-alone option AC reactor (FR-HAL) is not required. The DC reactor (FR-HEL) cannot be connected.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A701