• No : 21011
  • Release Date : 2018/08/22 16:25
  • Print

FR-A701

Can I connect the reactor for the harmonic suppression to the FR-A701?
Category : 

Answer

The AC reactor (FR-HAL) is built in the FR-A701. (The circuit type in the Harmonic Suppression Guidelines is three-phase bridge (capacitor smoothed), with reactor (AC side).) The connection with the stand-alone option AC reactor (FR-HAL) is not required. The DC reactor (FR-HEL) cannot be connected.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A701