- No : 21030
- Release Date : 2018/08/22 16:25
-
Print
FR-F700PJ
Is "F" written in the model on the plate of the product with filterpack?
- Category :
-
Answer
To indicate that the filterpack is included, "F" is written in the packaging plate. However, "F" is not written in the inverter rating plate because the standard inverter and inverter with filterpack are the same.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F700PJ