• No : 21030
  • Release Date : 2018/08/22 16:25
  • Print

FR-F700PJ

Is "F" written in the model on the plate of the product with filterpack?
Category : 

Answer

To indicate that the filterpack is included, "F" is written in the packaging plate. However, "F" is not written in the inverter rating plate because the standard inverter and inverter with filterpack are the same.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-F700PJ