- No : 21053
- Release Date : 2018/08/22 16:25
-
Print
Safety stop function
There are connection diagrams that the safety relay module is connected to the multiple inverters. How many inverters can be connected to the safety relay module?
- Category :
-
Answer
Up to three inverters can be connected. When more than four inverters are connected, the inverters may not be recognized because of the voltage drop.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800