• No : 21068
  • Release Date : 2018/08/22 16:25
  • Print

Sine wave filter

When using Real sensorless vector control, can I use the sine wave filter?
Category : 

Answer

The sine wave filter can be applied only under V/F control. When Pr.72 PWM frequency selection is set to 25, V/F control is set automatically. The applicable output frequency is 60 Hz or less.
Product Name
Inverter, magnet motor drive
Product Category
Option
Series
FR-A800, FR-A700