• No : 21077
  • Release Date : 2018/08/22 16:25
  • Print

Installation necessity of a DC reactor

What is the condition where a DC reactor connection is required?
Category : 

Answer

A DC reactor connection is required under the following conditions.
- Inverter capacity is 75K or higher - Motor capacity is 75 kW or higher. If any of the above conditions is met, always connect a DC reactor.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800, option