- No : 21089
- Release Date : 2018/08/22 16:25
-
Print
Wiring length
In the FR-A700/F700P, the maximum wiring length is 100 m when the shielded cable is used. Is it changed in the FR-A800/F800?
- Category :
-
Answer
In the FR-A800/F800, the restriction on the wiring length of the shielded cable is eliminated. The wiring length is up to 500 m as is the case with the unshielded cable.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800