- No : 21095
 
      - Release Date : 2018/08/22 16:25
 
        - 
          
              Print
          
        
 
  
 
USB
    
      What is USB used for?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    The mini B connector is used for connecting with FR Configurator2. A USB memory device can be connected to the A connector (host) to save parameters or trace data or to copy parameters from one A800/F800 to another A800/F800. Parameters can be copied from one to another through a USB cable connected to the A connectors.
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Inverter
 
      
      
        - Series
 
          - FR-A800, FR-F800