- No : 21101
- Release Date : 2018/08/22 16:25
-
Print
Multiple rating
What are the advantages by the multiple rating?
- Category :
-
Answer
By setting the operating condition, such as load level and surrounding air temperature, according to the application, the inverter capacity may be lowered compared to the conventional model depending on the conditions, allowing installation space to be minimized and costs reduced.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800