• No : 21109
  • Release Date : 2018/08/22 16:25
  • Print

FR-A800

Is the installation compatible with the A700 series? FR-A720-0.4K to 90K, FR-A740-0.4K to 280K, FR-A740-315K to 500K
Category : 

Answer

- The 280K or lower has the installation size compatibility. - The 315K or higher does not have the installation compatibility; because the inverter unit and converter unit are separated. For the details of installation size, refer to the catalog.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800