• No : 21112
  • Release Date : 2018/08/22 16:25
  • Print

DC reactor

A DC reactor is not enclosed. Is no DC reactor required if harmonics are suppressed by other means than inverter reactors?
Category : 

Answer

If using an inverter with capacity of 75K or higher, or motor with capacity of 75 kW or higher, always select and install the inverter based on the capacity of the motor with DC reactor.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800