• No : 21185
  • Release Date : 2018/08/22 16:26
  • Print

Brake sequence function

The instruction manual includes the following description: "Set the acceleration/deceleration time to 1 s or more". What is the corresponding value (Hz) to 1 s?
Category : 

Answer

The value of Pr.20 (Acceleration/deceleration standard frequency) is corresponding to 1 s. (Initial value: 60 Hz)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700