- No : 21208
- Release Date : 2018/08/22 16:26
-
Print
Cumulative energization time
Is cumulative energization time accumulated on the monitor even when only the control power is ON?
- Category :
-
Answer
It is accumulated even when only the control power is ON.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700