• No : 21208
  • Release Date : 2018/08/22 16:26
  • Print

Cumulative energization time

Is cumulative energization time accumulated on the monitor even when only the control power is ON?
Category : 

Answer

It is accumulated even when only the control power is ON.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700