• No : 21215
  • Release Date : 2018/08/22 16:26
  • Print

Parameter copy

It is described that parameter copy in the FR-A700 and FR-F700(P) with the DU07 should be performed while the inverter is stopped. What happens if it is performed during the operation?
Category : 

Answer

Reading during the operation is possible. However, when writing is performed during the operation, "rE2" (parameter write error) occurs.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700, FR-F700P, FR-F700