• No : 21218
  • Release Date : 2018/08/22 16:26
  • Print

Torque limit

When performing the torque limit of the speed control, are Pr.816 (Torque limit level during acceleration) and Pr.817 (Torque limit level during deceleration) valid if Pr.815 (Torque limit level 2) is set, TL (torque limit selection) signal is turned ON, and the second torque limit is used?
Category : 

Answer

When the second torque limit is used, the settings of Pr.816 and 817 are valid.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A700