• No : 21222
  • Release Date : 2018/08/22 16:26
  • Print

System environment variable of the Modbus-RTU communication

How does the system environment variable 40009 (control input command) operate when 0 bit (stop command) is turned ON?
Category : 

Answer

It decelerates and stops. The operation is the same as the one when the Bit of forward rotation command and reverse rotation command are turned OFF.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700