• No : 21223
  • Release Date : 2018/08/22 16:26
  • Print

System environment variable of the Modbus-RTU communication

Are system environment variable 40003 (parameter clear) and 40004 (all parameter clear) available during the operation?
Category : 

Answer

They are not received during the operation. They are also not received if the command authority does not exist in the communication. When they are executed in the NET operation mode, "E.PUE" occurs and the inverter trips.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700