- No : 21224
- Release Date : 2018/08/22 16:26
-
Print
System environment variable of the Modbus-RTU communication
In the Instruction Manual, it is described that the writing value is optional for system environment variable 40002 (inverter reset). Is any kind of numerical values can be input?
- Category :
-
Answer
Other than "0" can be input. The inverter is reset by writing any numerical value.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700