• No : 21349
  • Release Date : 2018/08/22 16:27
  • Print

Operation panel and FR-PA07

Can I use both the operation panel of E/D700 and FR-PA (PU)07 (PU connector connection)?
Category : 

Answer

Since the operation panel and PU connector cannot be specified for command source at the same time, they cannot be used together.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ