• No : 21354
  • Release Date : 2018/08/22 16:27
  • Print

Operation mode setting

When Pr.79 (Operation mode selection) of the inverter is set to "3", operation is not changed by changing the setting of Pr.275 (Stop-on contact excitation current low-speed multiplying factor). What are the possible causes?
Category : 

Answer

The stop-on-contact control does not function in the combined operation mode.  

Perform the control in the External operation mode.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700