• No : 21367
  • Release Date : 2018/08/22 16:27
  • Print

FR-PA02

Can I use the operation panel used in the FR-E500 by setting Pr.146 (Built-in potentiometer switching) to "0"?
Category : 

Answer

The operation panel FR-PA02 requires the optional FR-E5P (control panel rear cover and adapter set) and connection cable FR-CB20□.
Check that Pr.146 (Built-in potentiometer switching) is set to "0".
Otherwise, the built-in potentiometer of the FR-PA02 cannot be used.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ