• No : 21421
  • Release Date : 2018/08/22 16:27
  • Print

Built-in reactor

Why is it necessary to build in the reactor?
Are the specifications of the built-in reactor same as the FR-BAL?
Category : 

Answer

The reactor built in the FREQROL-A201 series is intended to stabilize operation of the converter circuit and differs from the FR-BAL. Note that when performing calculations given in the harmonic suppression guidelines, use the conversion coefficient of K31 = 3.4 (no reactor) because the built-in reactor does not have a sufficient harmonic suppression effect.
Product Name
Inverter, magnet motor drive
Product Category
Power factor improving reactor
Series
Option, others