- No : 21501
 
      - Release Date : 2018/08/22 16:27
 
        - 
          
              Print
          
        
 
  
 
Inverter analog output
    
      I want to input two channels each from the inverters FR-B-37K (with parameter unit), FR-B-5.5K (with parameter unit), and FR-B-1500 (with parameter unit) (all based on the FR-A220E) to the programmable controller as the analog monitor. Which option do I need? Or, can I do this without any option?
    
  
    - Category : 
 
    - 
      
    
 
  
 
    Answer
  
    Since the inverter has only one voltage output (10 VDC) from terminal AM as the analog monitor, use the FR-EPA or FR-EPE option if you need two channels. 
The FR-EPA and FR-EPE options have the voltage output (5/10 VDC) × 1 and current output (1 mA DC) × 1 that can be used simultaneously. 
Use one of the above options, and determine if you use two channels from the option or one channel each from the inverter and option.
  
    
      
        - Product Name
 
          - Inverter, magnet motor drive
 
      
      
        - Product Category
 
          - Others
 
      
      
        - Series
 
          - FR-B