- No : 21543
- Release Date : 2018/08/22 16:28
-
Print
Torque characteristic at low speed
The catalog indicates the speed control range without PG as 1:120 (0.5 Hz to 60 Hz power driving).
What are the speed fluctuation rate and torque characteristics at 0.5 Hz or slower?
- Category :
-
Answer
Torque is not guaranteed for slower than 0.5 Hz.
Therefore, no data for this is published. Also, no torque is generated at 0 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500