• No : 21543
  • Release Date : 2018/08/22 16:28
  • Print

Torque characteristic at low speed

The catalog indicates the speed control range without PG as 1:120 (0.5 Hz to 60 Hz power driving).
What are the speed fluctuation rate and torque characteristics at 0.5 Hz or slower?
Category : 

Answer

Torque is not guaranteed for slower than 0.5 Hz.
Therefore, no data for this is published. Also, no torque is generated at 0 Hz.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A500