- No : 21563
- Release Date : 2018/08/22 16:28
-
Print
Regenerative driving capability
How much is the regenerative driving capability?
- Category :
-
Answer
Continuous 100% regenerative braking torque is available for the rated capacity of the high power factor converter. (The same braking ability of the FR-A201 inverter with the built-in power supply regenerative function is achieved.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option