• No : 21563
  • Release Date : 2018/08/22 16:28
  • Print

Regenerative driving capability

How much is the regenerative driving capability?
Category : 

Answer

Continuous 100% regenerative braking torque is available for the rated capacity of the high power factor converter. (The same braking ability of the FR-A201 inverter with the built-in power supply regenerative function is achieved.)
Product Name
Inverter, magnet motor drive
Product Category
High power factor converter
Series
Option