- No : 21610
- Release Date : 2018/08/22 16:28
-
Print
Difference in purpose from FR-A200 series
What is the proper use of the FR-A024 series and FR-A200 series?
- Category :
-
Answer
Reference of proper use of each series is as follows:
- A024: When balance between size, performance, and cost is important.
- A200: When system configuration (plug-in option), high performance, and large capacity are required.
When actually choosing the inverter, carefully consider the required capacity and specifications.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024