- No : 21625
- Release Date : 2018/08/22 16:28
-
Print
Communication option
Can I use the communication option FR-CU01 with the FR-A200 (E)?
- Category :
-
Answer
You can remove the parameter unit FR-PU02 and install the FR-CU01 there.
However, since the interface for the parameter unit is used, the communication speed is lower than the computer link plug-in option.
Similarly to the FR-PU02, the FR-CU01 can be installed and removed while the inverter is powered ON.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Others
- Series
- FR-A200