• No : 21642
  • Release Date : 2018/08/22 16:28
  • Print

Automatic restart after instantaneous power failure

Is it possible to restart the inverter after power failure? (Is automatic restart after instantaneous power failure available?)
Category : 

Answer

The inverter has the automatic restart after instantaneous power failure function.
By setting Pr.61 to other than "9999", the encoder detects the speed of the inverter after the power restores and restarts it from the coasting speed.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-V200