• No : 21660
  • Release Date : 2018/08/22 16:28
  • Print

New function of EXCELLENT

What are the new function of the A100E compared with the A100?
Category : 

Answer

The new function includes:
- PI control function
- Cumulative energy monitor (monitor accuracy: approximately ±25% of full scale value)
- Response current limit operation is improved.
- Extended carrier frequency setting range (0.7 to 14.5 kHz)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A100