- No : 21660
- Release Date : 2018/08/22 16:28
-
Print
New function of EXCELLENT
What are the new function of the A100E compared with the A100?
- Category :
-
Answer
The new function includes:
- PI control function
- Cumulative energy monitor (monitor accuracy: approximately ±25% of full scale value)
- Response current limit operation is improved.
- Extended carrier frequency setting range (0.7 to 14.5 kHz)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A100