• No : 21693
  • Release Date : 2018/08/22 16:28
  • Print

PU operation

I am using the inverter in the PU operation mode.
When I press the "RUN" key on the operation panel, the inverter rotates forward. How can I have it rotate in reverse when I press the "RUN" key?
Category : 

Answer

Set Pr.40 (RUN key rotation direction selection) to "1" (Reverse).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ