• No : 21698
  • Release Date : 2018/08/22 16:28
  • Print

FR-PA07

By connecting the optional FR-PA07, can I use both the inverter operation panel and FR-PA07?
Category : 

Answer

Basically it is not possible due to the operation command source.
However, if Pr.77 (Parameter write selection) is set to "2", you can use both the FR-PA07 and the inverter operation panel to set parameters.
Note that you can switch between forward and reverse rotation from the FR-PA07 only.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ