- No : 21699
- Release Date : 2018/08/22 16:28
-
Print
FR-PA07
When the optional FR-PA07 is connected, does the inverter operation panel turn off?
- Category :
-
Answer
Only the operation command source is switched to the FR-A07 and the inverter operation panel does not turn off. (Setting from the inverter operation panel becomes unavailable.)
However, if Pr.551 (PU mode operation command source selection) is set to "2" (PU connector is the command source) and Pr.77 (Parameter write selection) is set to "2", you can use both the FR-PA07 and the inverter operation panel to set parameters.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ