• No : 21703
  • Release Date : 2018/08/22 16:29
  • Print

FR-PA07

I am using the optional operation panel FR-PA07 connected with a cable with Pr.79 (Operation mode) set to "3".
When using this FR-PA07 and external terminals, does the "RUN" key on the FR-PA07 work?
Category : 

Answer

No. The "RUN" key on the FR-PA07 does not work.
The start command is accepted from the external source.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ