• No : 21707
  • Release Date : 2018/08/22 16:29
  • Print

Terminal CS

I once used the FR-A500 series.
At that time, the terminals CS and SD were short-circuited for automatic restart after instantaneous power failure, does the FR-E700 series have the terminal CS?
Category : 

Answer

FR-E700, D700, and F700PJ do not have the terminal CS and you can only control automatic restart by setting Pr.57 (Restart coasting time).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ