- No : 21748
- Release Date : 2018/08/22 16:29
-
Print
Auto tuning
I performed offline auto tuning and "3" was shown on the monitor.
I checked the setting of Pr.96 (Auto tuning setting/status) by reading and it was "3".
I had set it to "1", but it changed to "3". Is it OK?
- Category :
-
Answer
When offline auto tuning ends normally, the setting of this parameter changes to "3".
This means that auto tuning completed normally.
If the setting value is "101", it changes to "103".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700