• No : 21752
  • Release Date : 2018/08/22 16:29
  • Print

Auto tuning

I use the geared motor GM-DZG. Which value should I set to Pr.71 (Applied motor) for auto tuning?
Category : 

Answer

Set it to "13" (Constant-torque).  
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-A700