• No : 21754
  • Release Date : 2018/08/22 16:29
  • Print

Advanced magnetic flux vector control

To perform Advanced magnetic flux vector control, I set Pr.71 (Applied motor) to "3", Pr.80 (Motor capacity) to "0.75 K", Pr.83 (Motor rated voltage) to "200 V", Pr.84 (Rated motor frequency) to "60", and Pr.96 (Auto tuning setting/status) to "1", but "1" is not shown when the screen returned to the monitor window.
What is wrong?
Category : 

Answer

Check the parameters necessary for tuning again.

Check if Pr.9 (Electronic thermal O/L relay) and Pr.81 (Number of motor poles) are set correctly.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700