• No : 21758
  • Release Date : 2018/08/22 16:29
  • Print

RS-485 communication

I want to perform RS-485 communication. 1. Is it correct to set Pr.117 for "n1" (Station number) of the FR-S500 for the D700/E700/F700PJ series?

2. Is it correct to set Pr.338, Pr.339, and Pr.342 for "n8" (Operation command source), "n9" (Speed command source), and "n12" (E2ROM write selection) of the FR-S500 for the FR-D700/E700/F700PJ?

3. Are there any other parameters to set?
Category : 

Answer

1. You can set Pr.117 for "n1" (Station number) of the FR-S500 for the D700/E700/F700PJ series.

2. You can set Pr.338, Pr.339, and Pr.342 for "n8" (Operation command source), "n9" (Speed command source), and "n12" (E2ROM write selection) of the FR-S500 for the FR-E700.

3. Change Pr.79 (Operation mode) to "2".
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ