- No : 21776
- Release Date : 2018/08/22 16:29
-
Print
Operation panel LED
I try to operate the inverter by inputting the start signal from the external terminal STF-SD and set the frequency using the setting dial.
For Pr.79 (Operation mode), "3" is set.
The operation panel LEDs "MON", "PU", "EXT", and "RUN" are lit. Is this OK?
- Category :
-
Answer
No problem.
LEDs "PU" and "EXT" indicate that Pr.79 is set to "3".
"MON" indicates that the operation status is monitored.
"RUN" indicates that the inverter is operating.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ