- No : 21782
- Release Date : 2018/08/22 16:29
-
Print
Frequency monitor window
While inverter running, pressing the "SET" key on the frequency monitor window allows for checking the voltage monitor. Also, the "Hz" lamp turns ON for the frequency monitor and the "A" lamp turns on for the current monitor.
When the key is pressed again, the "A" lamp turns off. Is this state the voltage monitor?
Now "19.5" is displayed.
- Category :
-
Answer
When both "Hz" and "A" are turned off, the output voltage monitor is active.
The display indicates that the output voltage is 19.5 V.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ